Sensors

Resources for Sensor Applications

Sensors Overview


A sensor collects and communicates critical data on its environment, ensuring safe, smooth, and efficient operation—and alerting when that isn’t the case. Whether it’s monitoring a vehicle’s engine or regulating the flow of oxygen to a patient, sensors help static components operate in a smarter manner. And growing technological trends, such as the Internet of Things and artificial intelligence, rely heavily on sensors to gather the data needed to carry out “smart” or autonomous capabilities such as assisted vehicle operation or automatic temperature adjustment. Looking ahead, sensors will need to be more adaptable than ever, with the ability to be packaged with other solutions and communicate wirelessly while operating with low-level power consumption and maintaining data integrity.

Transportation

Sensors serve as the crucial communication component between vehicle and operator, ensuring that vehicle functionality is performing as intended—as well as alerting and diagnosing when something isn’t right. Critical components of a vehicle, such as automated transmissions, engines, clutches, and brakes, are monitored by sensors for performance and safety purposes, ensuring a secure and enjoyable travel experience.  Today, vehicle sensors have expanded beyond monitoring baseline operations — they increasingly contribute to passenger comfort, emissions reduction, and power train improvement. Sensors in vehicles must be able to perform in harsh environments, with the ability to endure temperature, vibration, and shock stressors. And as vehicles increasingly embrace automated components, sensors are crucial for collecting and communicating data for safe handling on the road.

Industry 4.0

Industrial revolutions have signaled growth in manufacturing technologies over time, from mechanization to mass production to computers and automation. The emerging fourth industrial revolution is characterized by a combination of cyber and physical systems, fueled by breakthroughs in artificial intelligence, robotics, and similar technologies. Sensors have been a key component to this new wave of manufacturing, allowing for the automated monitoring of operations, equipment, and systems. Sensors can help improve predictive maintenance, asset monitoring, and process automation. And when it comes to factory-wide automation, valve and equipment data collection, diagnostics, and alerts through sensors are imperative to keeping operations in sync. Used in such environments, sensors must also be able to communicate seamlessly with each other and appropriate endpoints to ensure systemwide coordination. 

IoT

Smart, internet-connected devices range from consumer-level speakers and doorbells to enterprise-wide data collection, buildings, and response systems, and sensors are at the heart of them all. As the IoT industry continues to expand at a rapid rate — some $267 billion is expected to be spent on IoT by 2020, according to The Boston Consulting Group — sensors must continue to evolve. In order to work with the wide array of IoT devices, sensors must be able to adapt to offer multiple outputs, low-current consumption, and flexible, miniaturized packaging options. And Bluetooth and other wireless solutions are increasingly being paired with sensors to offer even more connectivity within the IoT environment.

Medical

A variety of sensors are used throughout the medical world, whether it’s to regulate and operate medical systems and devices or to monitor an individual. Sensors used for medical purposes are held to high standards and must provide unassailable accuracy and repeatability while meeting exacting specifications, including ISO 13485 certification and FDA registration. Medical equipment relies on sensors to control activity — such as using pressure sensors to place a patient under anesthesia—as well as accurately provide data to help diagnose and conduct treatment.

Specific sensors, such as air bubble detectors and biomedical sensors, are used primarily for medical purposes. However, sensors with broader capabilities are increasingly being paired with analytic technologies to build “smart” healthcare facilities. For example, infrared sensors can be used to monitor a patient’s activity — such as whether they are in bed or walking about the room — while respecting privacy and abiding by healthcare privacy laws. 

Featured Suppliers