Electric Vans Connected to Fleet Charging Stations

Electric vehicle charging systems are becoming more powerful, more complex and more interconnected, which means EMC can no longer be treated as a secondary design concern. As charging infrastructure expands and power levels continue to climb, EMC has a direct impact on whether a charger performs reliably in the field, communicates consistently and holds up under real operating conditions. Engineers who treat EMC as an afterthought often create avoidable problems that show up later in testing, deployment or long-term performance.

The reality is that EV chargers operate in an electrically demanding environment. High-frequency switching, power conversion noise paths, external noise coupling and even cable and connector behavior can all contribute to EMI issues that affect the overall system. These are not isolated effects. They influence how the charger interacts with the grid, how internal electronics behave and how reliably communication functions perform during operation. EMC touches all of it.

Where EMI Comes From

One of the biggest EMC challenges in EV charging is the amount of high-frequency activity built into the system itself. Modern chargers rely on fast-switching power electronics to achieve the efficiency and power density the market expects. That performance matters, but it also creates noise that must be controlled. The more advanced the charging architecture becomes, the less tolerance there is for weak EMC design.

In practice, EMI does not stay neatly contained. It can conduct back onto the grid, couple into adjacent circuits or interfere with communications inside the charger. Noise can move through intended and unintended paths, which is why layout, interconnect choices and cable behavior matter as much as the major electrical building blocks. I think this is where strong designs separate themselves from marginal ones. A charger may meet its core electrical targets on paper, but if its electromagnetic behavior is unstable, that weakness eventually surfaces.

Building EMC into the System

The most effective approach is to build EMC into the charging system from the start rather than trying to correct for it later. Input EMI filters are a foundational part of that strategy because they reduce conducted emissions before noise reaches the grid. Common-mode chokes, differential-mode inductors and capacitors each play a specific role in suppressing unwanted noise and improving overall system behavior. These components are not just supporting hardware. They are part of what allows the charger to operate as intended.

Protection is just as important. EV charging systems are exposed to surges, startup stress and transient conditions that can damage sensitive electronics if those risks are not managed correctly. Surge protection devices such as MOVs and TVS diodes help clamp voltage spikes. Inrush current limiters such as NTC and PTC thermistors help control startup conditions. Fusing adds another level of fault protection. From my perspective, these are the kinds of details that determine whether a charger is merely functional or truly robust.

Shielding and grounding also need to be treated as design priorities, not cleanup measures. Cable shielding, conductive enclosures and effective grounding strategies all contribute to reducing noise coupling and stabilizing operation. When they are approached as part of a coordinated EMC plan, the payoff is tangible: fewer failures in noisy environments, stronger protection for sensitive electronics, more reliable communications and more consistent charging uptime. Those outcomes matter because charger performance is ultimately judged in the field, not just in development.

What’s changing?

The EMC challenge is growing as the industry evolves. Higher-power charging, including 350 kW and above, increases the electromagnetic demands placed on the system. Wireless charging introduces added concerns around magnetic field leakage. Vehicle-to-grid architectures add bidirectional power flow, which expands the number of operating conditions designers have to account for. On top of that, the adoption of SiC and GaN devices is pushing switching speeds higher and moving EMI concerns into even more demanding frequency ranges.

That combination of trends makes one thing clear: EMC design is becoming more critical, not less. Regulatory frameworks will continue to matter, but compliance alone is not the full objective. The broader goal is system stability, resilience and charging consistency under real-world conditions. The strongest EV charging designs will be the ones that account for EMC early.

Follow TTI, Inc. on LinkedIn for more news and market insights.

Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Specialists.

Follow TTI, Inc. - Europe on LinkedIn for more news and market insights.

Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Specialists.


Gabe Osorio

Gabe Osorio

Gabe Osorio is a Director, with TTI, Inc.’s Transportation Business Unit. He has ten years of experience in the electronic components industry and has spent the last four years focused on tracking developments in electric vehicle technology. He provides connectivity solutions for power storage, distribution and charging in the transportation EV market.

View other posts from Gabe Osorio.
Latest Articles
MarketEYE Articles

View All Supply Chain Articles
Select Contributor to view their article(s)

View All Connector Articles
Select Contributor to view their article(s)

View All Passive Articles
Select Contributor to view their article(s)

Listen to our new podcast, TTI Distribution Download! TTI Specialists, supplier partners and more share their expertise and insight on the electronics industry. 

Apple | Spotify | YouTube

Stay Updated