Industrial IoT
Building a Secure, Connected Future
The Industrial Internet of Things (IIoT) impacts every aspect of industry. Manufacturing is becoming more efficient and products are easier to customize. Procurement and warehousing are smarter and less reliant on human intervention. Logistics systems can adapt to changing conditions and avoid costly supply chain disruptions. With capable, connected sensors and real-time data, you have countless opportunities to create innovative new solutions. Our IIoT Specialists are here to help, with knowledge and technology to make digital transformations seamless and successful.
Predictive Maintenance
Sensors have long been used to monitor critical components for failure—whether it’s on an airplane, in a valve, or along the production line—but today’s smart sensors can anticipate failures long before they occur. Predictive maintenance can be carried out in a variety of ways—the status of every connected machine is stored in one system, and a detailed history of each operational component is monitored. Performance improvements can be automatically calculated and scheduled based on the maintenance history of each individual machine.
Impending failures can also be detected in real-time by sensors that can monitor property changes far more accurately than humans. The slightest change in temperature, pressure, vibration, or decline in performance can be identified by sensors long before it becomes a catastrophic failure that could lead to downtime. Incredibly sensitive and reliable sensors are required for predictive maintenance—they must be able to detect the smallest change and communicate it in real-time, without fail.
Asset Monitoring
Sensors have long been used to monitor critical components for failure—whether it’s on an airplane, in a valve, or along the production line—but today’s smart sensors can anticipate failures long before they occur. Predictive maintenance can be carried out in a variety of ways—the status of every connected machine is stored in one system, and a detailed history of each operational component is monitored. PerforInternet-connected RFID tags, paired with sensors, are a game-changer to the logistics and supply chain industry, creating simple, low-profile solutions to tracking valuable goods from production to delivery and beyond. Sensors can monitor everything from raw material inventory to a finished product’s journey from the factory to the warehouse to the buyer, reducing delays in manufacturing and loss percentages during transport.
The combination of RFID tags, sensors, and internet-connected RFID readers has proved to be extremely valuable for many industries, including remote vehicle fleet management. RFID tags track the location of a vehicle, while sensors gather data about speed, vehicle maintenance, and more. This information is collected by an RFID reader, which sends it to a centrally-located network that can be easily monitored.
Building Automation
Internet-connected facility utilities allow for centralized and programmable control that automates building management for more power efficiency and savings. Connected sensors can monitor changes in a building’s environment and trigger changes in air conditioning, humidity control, lighting, access control, and more. Pressure and temperatures sensors and switches are especially important in monitoring HVAC systems, allowing for accurate and precise temperature control that ensures personal comfort and optimal machinery and factory operations.
Connected sensors can also help build a robust security and access control program throughout a facility. Such programmable sensors, paired with access control cards, can determine who can or cannot enter certain sections of a building. They can also help with lighting and elevator efficiency during peak or off-hours, creating a secure yet power-saving environment.
Process & Control Automation
According to recent research, the industrial robotics market is expected to grow by 175 percent over the next decade. And while robotic operations may be nothing new in factories, the addition of smart sensors plugged into a network will take mechanical operations to the next level by collecting valuable data about processes and controlling them remotely. Connected components can collect and analyze information about process flow, diagnostics, downtimes, inventory tracking and more—and action can be taken remotely via IoT solutions.
Connected sensor networks can make data collection more consistent, accurate and safe. Replacing dial gauges—especially those in hazardous or hard-to-reach areas with sensors, allows valuable data to be collected and sent straight to mobile devices. Such sensors must be rugged, reliable and able to operate in harsh environments to avoid machinery downtime or inaccurate readings. Additionally, incorporating machine learning programs into the data collection allows automated analysis based on the readings, which facilitates real-time, ongoing process correction as needed.
Transportation
Already widely available in consumer cars and transport fleets alike, IoT connectivity in vehicles has been a game-changer when it comes to navigation, asset tracking, safety, and efficiency. Internet-connected sensors built into vehicles can monitor location, speed, fuel consumption and more, making the logistics of product transport throughout an entire fleet easy to track and adjust via one centralized portal.
While still in the early stages of being adopted, fully connected and autonomous vehicles mark the precipice of a turning point in supply chain management. Vehicle-to-infrastructure and vehicle-to-vehicle communication capabilities will make shipping logistics safer and more efficient through automated route and navigation information, monitored cargo conditions, and predictive maintenance alerts—valuable information that can be constantly broadcast to a mobile device and analyzed.
Often referred to as the Fourth Industrial Revolution, the Industrial Internet of Things (IIoT) is the combination of physical machinery with Internet-connected software and sensors. The combination of cyber and physical systems within the industrial sector relies on sensors to gather huge amounts of data—from factory conditions to the health and operation of machinery to tracking individual components along the supply chain. This valuable data is transmitted to networks and often uses software to analyze and act on the data collected in real-time. This constant connectivity—and the insights provided by automated data analysis—will lead to more efficient operations and enable new, lower-cost solutions. Estimates show that by 2020, there will be more than 26 billion connected devices—a 30-fold increase in the connectivity available today. Many industries are benefitting from an IIoT approach, and more adopt connected solutions every day.
Factory Floor
Automation on the factory floor isn’t new, but connected sensors can gather valuable data that, when analyzed, can provide important assessments and insights that will keep operations running smoothly. Predictive maintenance is especially valuable—sensors can detect potential mechanical failures long before humans can, keeping machinery in peak shape without unexpected downtime.
Aerospace and Defense
The aerospace and defense industries have benefitted greatly from IIoT. Real-time data collection and analysis is crucial to both maintaining the operations of high-performance systems and informing tactical commands and decision making. Sensors must operate and communicate at 100 percent accuracy at all times, even in rugged conditions.
Transportation
Connectivity has already begun to infiltrate the transportation sector, with vehicle tracking, navigation and even driving assistance. When it comes to supply chain management, IIoT can assist with all of these components while tracking the location, temperature and the condition of assets being transported, ensuring efficiency and safety while reducing loss.
Medical
Patients and doctors alike benefit from a more connected medical system. Surgical systems, imaging and treatment machines, and connected medical devices can more easily communicate with each other, leading to safer, more customizable treatments and valuable insights to the care team.
All of these applications rely on reliable, rugged and connected sensors. Crucial to data collection are connectors with high-quality signal transmission, data flow, and power distribution. As more industries benefit from IIoT, components will have to be able to accommodate more bandwidth and speed to ensure peak performance.