Harsh Environments

Resources for Applications in Extreme Conditions

Today’s electronics are being used in harsher and more rugged environments than ever, facilitating new ways to operate in extreme conditions while keeping workers safe. Electronics used in harsh environments must be able to withstand extreme temperature and humidity, dust, electromagnetic interference, marine environments, and more, while operating at full capacity and without degrading. TTI carries a full line of durable components developed to perform in extreme conditions such as the heat and corrosion found at the bottom of an oil well or the temperature cycles and vibration in a jet engine.

Components used in harsh environments are manufactured to meet industry standards, including NEMA ratings and the IP Code (IEC 60529), and often surpass military- or space-level specifications. Take some pressure off your next design and call a TTI product specialist at 1.800.CALL.TTI to learn how our broad and deep inventory takes the heat.

IP Ratings

The IP (Ingress Protection) Code, which is defined by the International Electrotechnical Commission (IEC) under the IEC 60529 standard, designates the various types and degrees of protection afforded to electrical equipment by its enclosure. The requirements for each degree of protection, along with testing and confirmation procedures, are specified in the standard.

When it comes to code conversions, it is not possible to obtain an equivalent NEMA enclosure type from an IP code because NEMA types are tested over a wider set of environmental conditions. Converting a NEMA type to an IP code may provide a good line, but such conversions should always be verified by test.

NEMA Ratings

Like the IP Code, the National Electrical Manufacturers Association (NEMA) provides a popular standard for protective enclosures used in harsh environments. NEMA 250 includes ratings for indoor and outdoor locations—both hazardous and nonhazardous—and covers a broader set of harsh conditions than the IP code. These conditions include ingress of water and foreign objects such as fiber or dust, as well as corrosive agents and gases. The table below provides a brief description of each level of protection, which NEMA specifies with a NEMA enclosure type number.

200⁰C+

Active or passive cooling is often used to keep components within operating temperature range in the presence of high temperatures, but in some applications this can be impractical. The downhole oil and gas industry, for example, is a primary consumer of high-temperature electronic components, especially as resources grow scarcer and deeper wells need to be dug. Today’s downhole applications must be able to withstand increasingly high temperatures as the geothermal gradient of deep wells puts equipment in an extreme environment. Components of such applications must be able to operate at temperatures over 200°C while operating at peak capability—equipment failures lead to costly rig downtime.

Vibration

Vibration in electronic equipment is a major contributor to system failure and other operating problems. While some vibration in electronics is normal—even if it’s only experienced during shipping and transportation—portable electronics need protection from more serious impacts, such as the shock of being dropped.

In many industrial and military verticals, vibration isolation is a crucial part of a product’s design. While modeling and analysis can help determine potential vibration levels, testing is needed to ensure reliability in harsh conditions. Advanced stress testing techniques, such as Highly Accelerated Life Tests (HALT) and Highly Accelerated Stress Tests (HASS), are often required to detect potential vibration issues that might occur during a military-grade product’s 20-year life span. These methods stress products beyond their specifications to identify both operational and destruct limits.

Featured Suppliers