Fort Worth, Texas – October 6, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is stocking Yageo/KEMET MIL-PRF-39003 Solid Tantalum Capacitors.
These KEMET tantalum through-hole capacitors are hermetically sealed, allowing them to be utilized in high-humidity environments. With a rugged construction, they are designed for miniaturized circuitry and well suited for coupling, bypass, filtering and RC timing circuits. The MIL-PRF-39003 has excellent stability as well as extremely low DC leakage current, dissipation factor and ESR/impedance over a wide temperature and frequency range.
The MIL-PRF-39003 is available in case sizes A, B, C and D with a capacitance range of .0047uF to 330uF at an operating temperature range of -55°C to +125°C. These military tantalum capacitors are available in failure rate options of: Graded – B, C, D and G Exponential – M, P, R and S.
For more information, visit KEMET M39003 Solid Tantalum Capacitors | TTI, Inc.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About KEMET Corporation
KEMET Corporation is a global supplier of electronic components with over 160 patents and world-wide manufacturing plants that are leading the advancement of the most cutting-edge electrical solutions. The company offers customers the broadest selection of capacitor technologies in the industry across all dielectrics, along with an expanding range of electromechanical devices, electromagnetic compatibility solutions and supercapacitors. KEMET provides solutions demanding the highest standards of quality, delivery, and service.