Fort Worth, Texas – November 29, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is the largest stocking distributor for the Vishay/Sprague 134D Series Wet Tantalum HI-TMP® (200°C) Capacitor. The 134D Series is a wet tantalum, high-temperature capacitor with a glass-to-tantalum hermetic seal for your -5°C to 200°C operation. With a high-capacitance offering of 10uf up to 1000uf, the 134D Series has axial leads with standard terminations of tin/lead (Sn/Pb) or 100 percent tin (RoHS-compliant) available. These capacitors are capable of withstanding a minimum 500-hour life test at a temperature of 200°C at the applicable derated DC working voltage.

The primary uses for the Vishay/Sprague 134D Series are industrial applications in a high-temperature/high-stress environment and in petroleum exploration.

View all Vishay products.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About Vishay
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors, passive electronic components and circuit protection devices that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.™ Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH).