Fort Worth, Texas – May 12, 2022 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of Switchcraft’s 12GHz UHD Video Patch Adapters from stock at TTI.

Switchcraft 12GHz UHD Video Patch Adapters provide 12GHz+ UHD performance and are compatible with HD or UHD signals. These adapters are compatible with the front-facing jacks on Switchcraft 12GHz patch panels. This compatibility allows connection via BNC or MicroBNC plugs instead of patch panels, providing more flexibility to video engineers. The BNC versions of these adapters are available in short and long options to allow usage in adjacent ports.

Target applications include broadcasting, media and video engineering, to name a few. Don’t forget that these are made in the U.S. and are in stock and available today.

To learn more, visit Switchcraft 12GHz UHD Video Patch Adapters from TTI, Inc.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com