Fort Worth, Texas – May 12, 2022 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of the ComboLock Wire-to-Board Connector System from Amphenol FCI. This system is a modular, reliable and compact hybrid wire-to-board connector system that saves space and allows for simpler assembly and cable management. ComboLock Wire-to-Board Connectors feature a hybrid 1.00mm pitch signal and 3.00mm pitch power configuration with an active latching feature. These devices have a nominal current carrying capacity of 10A/pin maximum for power and 1.5A/pin maximum for signals where power wire sizes range from 26AWG to 18AWG and signal wire sizes from 30AWG to 24AWG.
Typical applications include consumer, industrial and data solutions, to name a few. They are in stock and available today at TTI.
To learn more, visit ComboLock Wire-to-Board Connector System from TTI, Inc.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com