Fort Worth, Texas – March 29, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is stocking the Vishay Dale Components RCWPM Zero Ohm Jumper (Military M32159) Thick Film Chip Resistor.
Vishay’s Zero Ohm Military/High Reliability Resistor fully conforms to the requirements of MIL-PRF-32159 and comes with M (military grade) and T (space grade) reliability with 100 percent group A screening per MIL-PRF-32159. The termination style B is a tin/lead wraparound over nickel barrier with an operating temperature range of -65°C to +150°C. Products with space level failure rates are only offered in packaging codes with ESD overpack and labeling. These devices are available in these case sizes: 0302, 0402, 0502, 0505, 0603, 0705, 1005, 1010, 1206, 2010, 2208 and 2512.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Vishay
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors, passive electronic components and circuit protection devices that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.™ Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE(VSH).