Fort Worth, Texas – March 16, 2022 - TTI, Inc., a leading specialty distributor of electronic components, is stocking Vishay’s BC components VY1 EMI/RFI Suppression and Filtering Ceramic Disc, used for antenna coupling, line-to-line filtering (Class X) and line-to-ground filtering (Class Y). The capacitor consists of a ceramic disc that is silver plated on both sides. Connection leads are made of tinned copper-clad steel, having a diameter of 0.6mm and offered with straight or kinked leads. The VY1 Series is made of a flame-retardant epoxy resin in accordance with UL 94V-0 and is available in capacitance values of 10pF to 4700pF.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Vishay
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors, passive electronic components and circuit protection devices that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.™ Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH).