Fort Worth, Texas – June 10, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is stocking Vishay CSC Thick Film, Conformal Coated, Single In-Line Networks. The CSC Series offers isolated, bussed and dual terminator schematics available in three body heights with “A” profile at 0.195" (4.95 mm), “B” profile at 0.295" (7.50 mm) standard and custom “C” profile at 0.350" (8.89 mm).

The “A” profile is standard in pin sizes 4-12, which helps decrease assembly cost, offering a wide resistance range of 10 ohm to 2.2M ohm and a zero ohm jumper. Bulk packaging is standard with optional tube packing.

The CSC Series is applicable for commercial and industrial-grade applications. Military options are available in the MIL-PRF-M83401, “H” and “J” schematic.

View all Vishay products.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About Vishay
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors, passive electronic components and circuit protection devices that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.™ Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE(VSH).