Fort Worth, Texas – June 10, 2022 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of Switchcraft 157/157G 1/4” Strap Nut End-Pin Jacks from stock at TTI.

Switchcraft 157/157G 1/4” Strap Nut End-Pin Jacks offer the same trusted quality as a standard Switchcraft End-Pin Jack with the added functionality of a removable strap nut. These jacks are ideal for acoustic guitar applications, eliminating the need to drill a second hole into the instrument for an output jack, and include a handle and a cable clamp to ensure critical connections are protected and all hardware is included for easy installation. The 157/157G End-Pin Jacks feature a durable and copper alloy strap nut with nickel- or gold-plated options. Target applications include musical instruments and speaker connections, to name a few. They are in stock and available today.

To learn more, visit Switchcraft 157/157G 1/4" Strap Nut End-Pin Jacks | TTI, Inc.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com