Fort Worth, Texas – June 1, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is stocking Knowles StackiCap™ X7R MLC Capacitors. Knowles’ unique, patented construction combined with FlexiCap™ terminations allow for high CV in compact packages. These capacitors are available in 1812-3640 case sizes and up to a 5.6uF, as well as 2KV in the X7R dielectric. Not only is its reduced PCB real estate an advantage, but these FlexiCap™ MLCCs can also withstand temperature cycling from -55°C to +125°C in excess of 1,000 times without cracking. Knowles offers specific ranges with the AEC-Q200 qualifications.
The StackiCap™ MLC Capacitor is suitable in a range of applications including power supplies, lighting, aerospace, electronics and high voltage applications where a large amount of capacitance is required.
To learn more, visit StackiCap™ Surface Mount MLC Capacitors | TTI, Inc.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Knowles
Knowles Syfer (formerly Syfer Technology Limited) is a premier global source for application specific multilayer ceramic capacitors and EMI suppression filters. Our comprehensive product range includes many application-specific capacitors, including FlexiCap™ and the new StackiCap™ range, as well as standard voltages and capacitance values.