Fort Worth, Texas – January 18, 2022 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of AICC’s 0.50mm Power Pin Floating Board-to-Board Connectors from TTI.
Amphenol ICC offers 0.50mm Power Pin Floating Board-to-Board Connectors in the B329/B322/B324/B326/B328 product series. These connectors are designed for applications that need large-current capacity and a space-saving design. The independent power pin supports 5A current per pin (power pin*4) and provides a high-speed data transmission performance of up to 10Gb/s. Key features include 10Gb/s high-speed transmission, current rating up to 5A per power pin (5A/pin* 4), a wide operating temperature from -55°C to +125°C (including T-Rise), a large floating range (X, Y ±0.60mm and Z ±0.50mm), anti-fool mating design and direction guide functions for easy mating.
These connectors are suitable for a wide range of applications across transportation, IoT, computing, industrial and medical markets, to name but a few. TTI offers a large inventory in stock today.
You can see more at 0.50mm Power Pin Floating Board-to-Board Connectors | TTI, Inc.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com