Fort Worth, Texas – January 17, 2022 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of Molex Micro-Fit+ Single Row Power Connectors with positive lock, right-angle headers and gold terminals from stock at TTI.
Molex has now added a single row receptacle and header to the range on Micro-Fit+. The Micro-Fit+ Connector is a wire-to-board system which offers a 3.00mm pitch, a higher-current rating of 12.5A and superior design options for flexibility and efficient assembly. The fact that the mating force is reduced by 40 percent over the standard Micro-Fit product, V-0/Glow Wire housings are standard and an enhanced TPA design is included makes this a great performing product.
Applications include consumer, medical, automotive/transportation and networking, to name a few. They are in stock and available today.
See more at Molex Micro-Fit+ Power Connectors | TTI, Inc.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com