Fort Worth, Texas – January 5, 2022 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of AICC’s Conan® Series Lite 1.00mm Connectors from TTI.
A secure, high speed and reliable board-to-board solution, Conan Lite 1.00mm Connectors come with a robust, metal down feature that helps in establishing a reliable connection with the PCB in both parallel and perpendicular board-to-board applications. These connectors also feature an audible “click” sound, ensuring mating is in place. Conan Lite vertical headers, receptacles and right-angle headers are offered in 9-69 positions and 4.15mm-7.5mm mating heights, making them suitable for a wide range of applications in the automotive, transportation, industrial and communications, to name but a few. They are in stock and available today at TTI.
To learn more, visit Conan® Series Lite 1.00mm Connectors at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com