Fort Worth, Texas – February 21, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is stocking Vishay’s T34 Wet Tantalum High Temperature Axial Lead Capacitor. Life tested at 200°C for 1000 or 2000 hours, these wet tantalums are excellent for down-hole drilling and extreme industrial applications.
The Vishay T34 has a tantalum case with a glass to tantalum hermetic seal. Rated at 70VDC at 200°C and 125VDC at 85֯°C with a capacitance range from 10uf to 680uf and a standard tolerance of 20 percent, the T34 is perfect for high temperature, high stress applications.
To learn more, visit T34 HI-TMP® Wet Tantalum Capacitor | TTI, Inc.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Vishay
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors, passive electronic components and circuit protection devices that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.™ Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE(VSH).