Fort Worth, Texas – February 15, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the G3VM High Current MOSFET Relay from OMRON. The G3VM-61GR2 features a continuous load current of 1.7A on a SOP-4 package with 80mΩ ON resistance, while the G3VM-61HR1 features a continuous load current of 3.3A (6.6A)* on a SOP-6 package with a low 30mΩ ON resistance. Typical application examples include metering, security, factory automation, industrial and medical.

To learn more, visit KEMET G3VM High Current MOSFETs at TTI.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com