Fort Worth, Texas – February 9, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the LN Series from Sensata, which feature panel mounted solid state relays that offer reliable, back-to-back SCR switching up to 75A at 528VAC, coupled with a patented trigger circuit design which allows the SSR to switch resistive loads with minimal electromagnetic noise generated. Ideal for use in commercial, residential and medical applications and UL recognized and TUV certified, the LN Series offers superior performance in applications that demand reliable switching and low emitted noise.
To learn more, visit Sensata LN Series Relays at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com