Fort Worth, Texas – February 9, 2022 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of Archer .8mm Board-to-Board Connectors from stock at TTI.
Harwin Archer .8mm Board-to-Board Connectors are compact and highly capable, micro-pitch connectors ideal for IIoT modules and embedded computing.
These connectors are designed for mezzanine daughterboard to motherboard layouts with an industrial-grade connection. The high pin counts on a .8mm pitch give a maximum PCB footprint of just over 50mm. The housing designs are polarized, and contacts are fully shrouded and protected to help prevent mis-mating and accidental damage to the contacts.
Archer .8mm Connectors have a surface mount design, are supplied in a tape and reel format with pick-and-place caps included and are ready for automated volume assembly. These board-to-board connectors are designed with location pegs to avoid movement before soldering and are ideal for E-vehicles, consumer electronics and industrial applications. They are used in a wide variety of applications including industrial, test & measurement, EVs, consumer and security, to name but a few. They are available today at TTI.
To learn more, visit Archer Board-to-Board Connectors | TTI, Inc.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Harwin
Harwin is a manufacturer of high reliability interconnects suitable for harsh environments and that are able to withstand extreme vibration, shock and temperature. Datamate, Gecko and M300 product lines have a proven history in Military, Aerospace and other safety critical markets. Other board level solutions include EMC Shielding products which increase reliability, flexibility and cost savings through the process of automated placement. Industry standard connectors and PCB hardware are also available from Harwin for commercial applications.