Fort Worth, Texas – August 10, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is the largest stocking distributor for Vishay QPL MIL-PRF-55342 Qualified Thin Film Surface-Mount Chip Resistors. These resistors feature all sputtered, wraparound termination for excellent adhesion and dimensional uniformity. These MIL-PRF-55342 qualified resistor chips are also ideal for applications requiring stringent performance requirements such as military, aerospace, satellites, handheld communication and just about anywhere that space is a premium. Established reliability is assured through 100 percent screening and extensive environmental lot testing per the QPL.

The MIL-PRF-55342 offers failure rates C, M, P, R, U, S, V and space level T. They are non-inductive, with laser trimmed tolerances +/- .1 percent and low noise. These high reliability QPL resistor chips are available in anti-static waffle pack or tape and reel packaging.

To learn more, visit: Vishay (MIL-PRF-55342) Thin Film Chip Resistor | TTI, Inc.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About Vishay
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors, passive electronic components and circuit protection devices that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.™ Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE(VSH).