A close-up of a large drill bit covered in dirt lies on the ground.

Walk into a design review for an oilfield project and you will often hear it: “Is it IP68?” But if you’ve spent time in the field, you know that is just the beginning. The real world is messier: connectors face temperatures that warp plastics, chemicals that eat seals, vibrations that shakes contacts loose, and electrical interference that can turn vital data into noise.

At TTI, we see the picture. We’re the ones who get the call when a “fully sealed” connector fails after six months in a sour gas environment, when a vibration-prone motor keeps losing signal, or when vital equipment puts you rig down because parts weren’t up to snuff. Our job is not to ship boxes, it is to help engineers avoid these headaches by matching their needs to the right solutions, with the documentation and spares to keep operations moving forward.

From Spec Sheet to Field Reality: The Questions That Matter

When a design engineer reaches out, the conversation quickly moves past catalog numbers. We ask:

  • What’s the worst this connector will see. Is it temperature, chemicals, vibration, pressure, or all of the above?
  • Is this a one-time install, or will techs be completing multiple mating cycles, in the rain, or with an ROV 2,000 meters down?
  • Is this part of critical operations and how challenging is redundancy (For the equipment or spare parts)?
  • What’s the cost of downtime if equipment fails?

The answers shape the conversation. For example, a “rugged circular” connector perfect for a control panel might be a disaster downhole where only a hermetic feedthrough will survive.  Meanwhile a seal that shrugs off Hydrocarbons might swell and crack in the presence of H₂S, causing failure of critical equipment. Each application will be shaped by the environmental conditions and how operators engage with the tool.

The Distributor’s Advantage: Seeing the Big Picture

Unlike a manufacturer, distributors see the full landscape, knowing which manufacturers are truly off-the-shelf, which are custom in disguise, which seal materials are in stock and which backshells actually fit the cable you’re using.

Let’s walk through a few real-world scenarios, and how we help engineers get from “problem” to “solution you can actually buy.”

An oil pumpjack is silhouetted against a bright blue sky with a few white clouds.

Scenario 1: The Topside Motor That Wouldn’t Stay Quiet

The Problem:
A land-based drilling operation kept losing clean sensor data from a mud‑pump drive motor. Though the connectors and cables meet all requirements for IP68 and published EMC guidelines, the field reality looked different. The variable frequency drive (VFD) on the mud pump was generating heavy harmonic noise, bleeding into sensor loops, intermittently tripping the control system, and halting drilling. After moving to backups and replacing multiple sensor replacements, the failures persisted.

The Fix:
We recommended an EMC-shielded circular connector (think: “E-Series”), paired with a 360° shield-termination backshell and a conductive gasket. The engineer ordered a bundle:

  • E-Series connector, size 18, 10-way
  • Matching backshell and gasket
  • FKM seal kit (for hydrocarbon resistance)
  • Dust caps
  • Cert pack with EMC and salt-fog test results

The Result:
The noise disappeared, and the maintenance team had spares and paperwork ready for the next audit.

Workers in a drilling operation are seen handling a pipe with heavy machinery.

Scenario 2: Downhole, Hermetics Only

The Problem:
A drilling‑tools manufacturer was qualifying a new measurement‑while‑drilling (MWD) tool designed to run in 200°C temperatures at 15,000 psi while sending real‑time gamma and directional data back to the surface. The tool needed a way to pass signals through a pressure boundary without compromising the integrity of the drillstring. For years, they had relied on an elastomer‑sealed feedthrough but extended thermal‑soak tests revealed seal creep and micro‑leaks the longer the tool stayed at temperature. In other words, the design worked at 150°C but not at the temperatures and pressures this next generation of wells required.

A leak here meant losing the tool downhole, expensive fishing operations, lost logging data and hundreds of thousands of dollars in downtime.

The Fix:
Once we reviewed the thermal and pressure requirements, it was clear the application had reached the limit of elastomeric sealing. We helped the team transition to a hermetic feedthrough, built with a ceramic insulator and compression‑sealed metal housing designed specifically for High Pressure and High Temperature (HPHT) boundaries. We bundled:

  • H-Feedthrough, 8-way, 200°C, 15k psi
  • Compression hardware
  • Service-side rugged circular connector (PEEK insulator, FKM seal)
  • Cert pack with pressure and leak test data


The Result:

With the new hermetic design, the feedthrough held steady through the full qualification matrix—no leaks, no drift, no surprises. The engineer could finally sign off on HPHT readiness, and the operations team appreciated having the spare feedthroughs and seals stocked locally. The tool entered field trials without redesign delays, and the project avoided the long lead time that often comes with custom HPHT components.

An oil rig stands in the ocean at dusk.

Scenario 3: Subsea, Where ROVs Rule

The Problem:
A subsea contractor was developing a sensor harness for a blowout preventer (BOP) control system on a deepwater installation. The harness linked position and pressure sensors on the BOP stack back to the umbilical termination module. This was critical equipment. Connector failure here compromised well-control systems.

During early qualification tests, the existing connector design showed leaks during pressure cycling, and ROV pilots struggled with alignment during underwater mating operations. Misalignment risks seawater intrusion and catastrophic failure for well-control infrastructure.

The Fix:
We supplied a wet-mate connector (“W-Connector” family), with pressure-balanced, oil-filled (PBOF) accessories and ROV alignment guides, designed specifically for subsea environments. The bundle included:

  • W-Connector, 6-way, NAB shell
  • PBOF kit
  • ROV stab-plate guides
  • Armor clamp
  • Spare seal set
  • Cert pack with submersion test results

The Result:
The ROV team could swap harnesses without flooding the system, and the spares were on the shelf. Long-term subsea deployment with reduced operational risk.

The Engineer’s Payoff: Fast Path from Problem to Solution

Here’s what makes a distributor’s approach different:

  • We ask about the environment, not just the part number.
    Is it hot/cold, are chemicals present, vibration, or is electromagnetic interference (EMI) likely? We’ll match you to the right material, seal, and finish.
  • We bundle everything you need.
    Connectors, backshells, seals, caps and certs—one order, one shipment, no surprises.
  • We offer alternates and spares.
    If there are concerns of delays we can design in redundancy with a second source. Then we ensure the spares you want are on our shelves, yours, or both.
  • We provide the paperwork.
    Need ATEX, IECEx, NACE, or RoHS? We’ll send the cert pack with your order.
A worker in a blue uniform and yellow hard hat stands near a large drilling rig.

What to Ask For: The Checklist

When you call or email, have these answers ready and elaborate on the application and requirements:

  1. What’s the worst environment application will face (Temperature, chemicals, vibration, EMC, pressure)?
  2. Is there a pressure boundary (hermetic)?
  3. Any special compliance needs (ATEX, IECEx, NACE, etc.)?
  4. How soon do you need it and how many spares?

We’ll do the rest:

  • Suggesting available options (with alternatives if needed)
  • Bundle the BOM: connector, backshell, seals, caps, and/or harness along with the required documentation.
  • Ship with the cert pack

Harsh‑environment work will always push equipment to its limits, and connectors are often where those limits show first. Thoughtful planning, clear documentation and a full view of the operating environment are what keep critical systems running when it matters most. The right questions, the right bundles and the right paperwork make all the difference.

Follow TTI, Inc. on LinkedIn for more news and market insights.

Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Specialists.

Follow TTI, Inc. - Europe on LinkedIn for more news and market insights.

Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Specialists.


Jim McNiel

Jim McNiel

The general manager of TTI, Inc.’s Houston, Texas branch, Jim McNiel has decades of expertise in supporting the electrical and electronic manufacturing industry. He is a graduate of Texas A&M University and has specialist experience in oil & gas exploration, among other industries.

View other posts from Jim McNiel.
Latest Articles
MarketEYE Articles

View All Supply Chain Articles
Select Contributor to view their article(s)

View All Connector Articles
Select Contributor to view their article(s)

View All Passive Articles
Select Contributor to view their article(s)

Listen to our new podcast, TTI Distribution Download! TTI Specialists, supplier partners and more share their expertise and insight on the electronics industry. 

Apple | Spotify | YouTube

Stay Updated