A blue sign labeled ZONE with a white Wi-Fi symbol is mounted on a pole.

Using current industry standards, WiFi can claim multi-gigabit throughput, sub-10 millisecond latency and packet loss rates below 0.1%. Nevertheless, future WiFi advances (upcoming 802.11be, known as WiFi 7 and WiFi 8  or 802.11bn) are shifting focus from raw speed to ultra-high reliability, AI-driven efficiency and even latency lowered by 25% compared to the Extremely High Throughput (EHT) MAC/PHY operation. EHT refers to the WiFi 7 standard designed to deliver at least 30Gbps, with higher reliability across 2.4, 5 and 6GHz bands,

With phones, laptops, wearables, gaming consoles and smart-home gear all online at once, all these connections are creating airtime congestion, lag and uneven performance. Even with WiFi's most capable bandwidth, sheer device density still causes latency spikes and slowdowns across the network. As enterprises increasingly rely on AI for critical operations and security, the demand for a robust, intelligent and secure network infrastructure has never been greater.

To meet these challenges, WiFi 8 is being created for launch roughly in 2028 to improve performance by a measurable amount. IEEE standard 802.11bn will serve as the foundation for WiFi 8, which is designed to support the future of connected technology. AI‑driven systems, busy mobile environments and immersive apps that demand ultra‑fast, interference‑resilient and coordinated connectivity.

What is more, in WiFi 8 new PHY and MAC layer technologies will work together to extend range, improve spectrum utilization, reduce latency and set the stage for ultra-high reliability (UHR) performance.

Meeting the Demands of Next-Generation Apps

With WiFi 8, users can expect much more than an upgrade in speed; they can expect a fundamental shift driven by market and end-user needs. For instance, the addition of Wireless Time-Sensitive Networking leveraging the precision of the IEEE 1588 Precision Time Protocol (PTP) provides the foundational technology for next-generation industrial AI. PTP is an IEEE standard network-based protocol designed for high-precision time synchronization, achieving sub-microsecond or nanosecond-level accuracy. It is critical for industries requiring tight synchronization, such as industrial automation, telecommunications, financial trading and audio/video broadcasts.

Other advances include multi-link operation for simultaneous band usage, coordinated beamforming to reduce interference and self-healing networks for stable, consistent connectivity in crowded environments such as industrial IoT, AR/VR and high-density public spaces.

WiFi 8 will support many types of DDR including DDR5/LPDDR5 and DDR4/LPDDR4 to enable OEMs to design in flexibility to react to the quickly changing commodity memory markets. WiFi 8 will further maintain backward compatibility with legacy devices while optimizing performance for next-generation, latency-sensitive applications.

Devices can stay connected farther from the router. With WiFi 8, when the signal weakens slightly, such as when moving farther from your router, the device won’t suddenly slow down causing lag or buffering.

The restriction of WiFi 6 (802.11ax), where each client is limited to a single resource unit (RU) per transmission, is removed in WiFi 7 through the introduction of multiple resource unit (MRU) support. MRU enables flexible spectrum utilization, significantly reducing latency and boosting overall system throughput.

Focus on Reliability

In previous generations of WiFi including WiFi 7, all spatial streams had to use the same modulation and coding scheme even when some streams had stronger signal conditions than others. A weak stream would slow the strong ones down.  Unequal modulation is a WiFi 8 feature that allows MIMO spatial streams to use different modulation and coding schemes based on individual signal quality, rather than forcing all streams to use the same, weakest-link rate.

Advanced 5x5 MIMO architectures (5-input, 5-output) will help Wi‑Fi 8 platforms deliver higher capacity and more reliable connectivity across a wider range of real‑world deployment scenarios. 5x5 MIMO technology uses five antennas to transmit and receive data, increasing spatial efficiency, data rates and connection reliability. It improves throughput, reduces congestion and enables faster, more consistent connectivity for high-bandwidth applications like extended reality (XR) – which includes virtual reality (VR), augmented reality (AR) and mixed reality (MR) – all of which require massive data throughput and extremely low latency to function effectively.

WiFi 8 extends the upper band limit from 7.125GHz to 7.25GHz. This shift enables the addition of one more 320MHz channel and another 160MHz channel – critical assets in reducing interference and enhancing performance in dense environments.

A Sneak Peek

While the WiFi 8 network does not exist yet, suppliers such as Qualcomm Technologies have developed a WiFi 8 portfolio sampling to customers now with first commercial products expected in late 2026.

Using the CMP180 radio communication tester from Rohde & Schwarz, Qualcomm Technologies recently completed validation and performance testing of its 5x5 radio technology designed for the WiFi 8 networking platform to validate advanced multi-antenna capabilities that are designed into its next-generation WiFi 8 platforms, including support for 5x5 MIMO in the 2.4, 5 and 6GHz band.

In all, the new feature set of WiFi 8 will accelerate the wireless LAN performance at home and in offices, venues and factories and enable applications like extended reality, AI-assisted applications, real-time cloud gaming and ultra-high-definition content streaming.

WiFi 8 will be purpose-built for the AI era – in smart homes, in businesses and even in crowded arenas. If you are using a WiFi 5 or WiFi 6 router, upgrading to WiFi 7 will get you to faster speeds, better coverage and lower latency, which helps with everything from 4K and 8K streaming to video calls. WiFi 8 speeds are the same as WiFi 7, but the real difference is consistency and responsiveness. It is being designed to deliver wired-grade reliability for mission-critical applications in enterprise, home and large-scale venues.

Follow TTI, Inc. on LinkedIn for more news and market insights.

Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Specialists.

Follow TTI, Inc. - Europe on LinkedIn for more news and market insights.

Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Specialists.


Murray Slovick

Murray Slovick

Murray Slovick is Editorial Director of Intelligent TechContent, an editorial services company that produces technical articles, white papers and social media posts for clients in the semiconductor/electronic design industry. Trained as an engineer, he has more than 20 years of experience as chief editor of award-winning publications covering various aspects of consumer electronics and semiconductor technology. He previously was Editorial Director at Hearst Business Media where he was responsible for the online and print content of Electronic Products, among other properties in the U.S. and China. He has also served as Executive Editor at CMP’s eeProductCenter and spent a decade as editor-in-chief of the IEEE flagship publication Spectrum.

View other posts from Murray Slovick.
Latest Articles
MarketEYE Articles

View All Supply Chain Articles
Select Contributor to view their article(s)

View All Connector Articles
Select Contributor to view their article(s)

View All Passive Articles
Select Contributor to view their article(s)

Listen to our new podcast, TTI Distribution Download! TTI Specialists, supplier partners and more share their expertise and insight on the electronics industry. 

Apple | Spotify | YouTube

Stay Updated