If you’ve been keeping up with market predictions about immersive graphics and accelerated AI you know that one thing is beyond question: memory will be increasingly important, powering innovation across both consumer and enterprise systems. Once limited to gaming consoles, graphics DRAM is now also supporting AI workstations and server GPUs with its higher performance and power efficiency.
Since its introduction in 2000, graphics double data rate (GDDR) has become the primary memory technology for graphics cards. GDDR memory is faster than DDR memory when it comes to bandwidth and data transfer rates. It is specifically engineered for graphics cards and GPUs, prioritizing high bandwidth to handle large volumes of data, such as high-resolution textures and 3D models. In contrast, DDR memory is optimized for general-purpose computing tasks managed by the CPU, focusing on lower latency rather than raw bandwidth.
GDDR7 is the next-generation graphics DRAM standard, delivering a jump in speed, efficiency and reliability for GPUs and AI accelerators. GDDR7 is suited for generative AI inference, autonomous driving and edge computing. It provides up to 192 GB/s of bandwidth per device –more than double that of its predecessors and well ahead of alternatives.
GDDR7 represents a significant upgrade over GDDR6. It certainly has its spec sheet right. The most notable difference is speed: GDDR7 delivers data rates of 32 Gbps per pin and can reach up to 48 Gbps or higher in future iterations, compared to GDDR6’s maximum of 24 Gbps. This results in up to 2x the bandwidth, enabling faster data access and processing for demanding applications.
GDDR7 is a JEDEC-approved open standard, ensuring broad industry support and interoperability. JEDEC published the GDDR7 standard in March 2024, with memory vendors reaching mass production this year.
By operating at a lower voltage (1.2V vs. GDDR6's 1.35V) and implementing a more efficient signaling method (PAM3, pulse amplitude modulation with 3 levels) GDDR7 enables higher data rates without needing a higher core clock speed. GDDR7 improves power efficiency by over 50%. This helps manage the thermal output of high-performance GPUs.
Several memory vendors including Samsung, Micron and SK Hynix are now in mass production of GDDR7 chips. NVIDIA has already chosen GDDR7 for its Blackwell-based RTX 50 series of consumer GPUs, providing a performance upgrade over its previous RTX 40 series. While NVIDIA was the first to ship consumer products with GDDR7, the new memory standard is expected to become commonplace across the industry. Samsung's 24Gb GDDR7 modules are integrated into NVIDIA's RTX PRO 6000 Blackwell Workstation and server GPUs, enabling up to 96GB of memory for complex AI workloads.
Compared to other memory types, GDDR7 stands out for its ability to efficiently feed data-hungry AI inference engines, enabling faster processing of large language models, real-time analytics and advanced edge applications.
Beyond consumer graphics, GDDR7 is also well-suited for high-performance computing at the "edge." However, it coexists with high bandwidth memory (HBM), a high-performance memory standard used in demanding applications like AI training and data centers, because it provides extremely high bandwidth and power efficiency through its 3D-stacked DRAM chips and wide interface. Unlike traditional memory, HBM uses a silicon interposer (a small substrate that acts as a-fast bridge between the memory chips and the main processor) to create a 1024-bit or wider data path, allowing it to transfer vast amounts of data faster.
But while HBM4 offers higher bandwidth and wider bus widths, it is significantly more expensive and complex to integrate. GDDR7 provides a cost-effective solution for applications that don't require HBM's extreme performance.
Similarly, LPDDR5 (low power DDR5) is optimized for energy efficiency and compactness, making it the memory of choice for mobile devices, laptops and other battery-powered systems. LPDDR5 typically supports data rates of 6.4–8.5 Gbps per pin, with a focus on minimizing power consumption. While LPDDR5 is highly efficient and supports reasonable bandwidth for mobile and embedded applications, it cannot match the raw speed and throughput of GDDR7, which consumes more power and is less suitable for compact, battery-powered devices.
In all, GDDR7 memory delivers significant improvements for AI inference workloads through advancements in bandwidth, efficiency and signaling technology and is well-suited for applications that require rapid movement of large amounts of data, such as real-time graphics rendering and AI model inference. It further makes it possible for compact systems to deliver data center-level performance in retail, healthcare and IoT.
Follow TTI, Inc. on LinkedIn for more news and market insights.
Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Specialists.
Follow TTI, Inc. - Europe on LinkedIn for more news and market insights.
Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Specialists.