fingers holding tools working on a transistor

The creation of the first transistor in December of 1947 sparked an evolutionary spiral that has forever changed our world. Evolving from a single gate on a chunk of germanium, engineers found ways to fabricate multiple devices on a common silicone substrate. 

Introduction of commercial transistor radios in the mid-1950s was a harbinger of how this new disruptive technology would alter expectations of electronic devices. No longer hobbled by the large size, excessive power and heat of a vacuum tube, electronic products could become smaller, lighter and energy efficient enabling powerful laptop computers and an entirely new class of mobile devices. 

Eighteen years later, Gordon Moore suggested that the number of transistors on a chip would double about every two years – a prediction that held true for over 60 years. Development of the integrated circuit in 1961 allowed the fabrication of multiple types of semiconductor devices including memory and passive components on a single die to create complex functional circuits. Advanced photolithography and deposition processes produced ever smaller devices on denser centerlines.  

Placing active devices in close proximity increases the number of devices per chip and wafer, allows greater device functionality while reducing the cost per chip. Shorter links between devices reduces latency allowing faster performance. Demand for more powerful computing capability in smaller envelopes touched off a race to shrink the transistor to near-atomic levels. 

The scaling of fabrication processes resulted in a continuous cycle of squeezing more transistors onto a monolithic die. The first multi-core processor chip was introduced by IBM in 2001 and was designed to simultaneously manage multiple processes more efficiently while consuming less power. With features measured in nanometers, the industry had achieved high volume production capability of devices with 32nm nodes by the late 2000s. 

Additional architectures including the development of the microprocessor, microcontroller, system-on-chip (SOC) and the three-dimensional IC enabled entirely new segments of the industry to flourish.  The result of these remarkable advances in device fabrication accelerated the ongoing revolution of electronic devices that pervades every aspect of our lives today.

After more than 50 years of miniaturization, the transistor and Moore’s Law may be nearing their technical and economic limits. As devices become more tightly packed, accumulating heat can build up to exceed maximum temperature specifications. Insulation between elements becomes so thin that current leakage becomes a problem. The wavelength of light used in the photolithography process is reaching limitations to create finer features.  

The decline in the curve of transistor dimensions has begun to flatten out, although engineers continue to find ways to increase the transistor count per die through advanced manufacturing processes including the use of extreme ultraviolet imaging technology.

Semiconductor processes improvements continued to advance with transistor dimensions shrinking from 32nm, 22nm and 14 nm.  Intel announced that it can pack more than 100 million transistors in each square millimeter of chip using its 10nm technology.  IBM announced a new 5nm process that would enable placement of up to 30 billion transistors on a chip the size of a human fingernail.  

Recent chip designs are being customized to support specific features or applications. Nvidia recently announced their Grace CPU, which is optimized for artificial intelligence calculations. A Korean AI chip designed for intelligent TV and voice recognition applications processes data at 40 trillion cycles per second while consuming reduced power.

The cost of building and equipping a state-of-the-art chip fab plant runs into billions, and a fab takes years to become operational. Very few companies can support that level of long-term investment. TSMC’s 5-nanometer technology will be utilized in a new facility slated to begin construction in Arizona. It is scheduled to produce 20,000 wafers per month by 2024. 4nm, 3nm and 2nm processes in development. TSMC has budgeted $100 billion for R&D and fab construction over the next three years. 

Research is underway to determine if it is physically possible and economically feasible to fabricate transistors by manipulation of individual atoms. A proposed government infrastructure spending bill includes earmarks of $50 billion for advanced semiconductor research and development. Some of those funds likely will be directed to study the feasibility of replacing electrons with photons in next generation silicon photonic chips, the next likely step in the evolution of semiconductor technology.

Follow TTI, Inc. on LinkedIn for more news and market insights.

Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Businesses.


Ronald E. Bishop

Ronald E. Bishop

Ronald E. Bishop founded Bishop & Associates Inc., a market research firm that specializes in the world electronic connector industry, in 1985. The firm publishes a monthly newsletter titled “The Bishop Report,” and a weekly digital publication from Connector Supplier.

Bishop & Associates’ research reports focus on connector sales by geographic regions, end-user equipment markets, connector products, and interconnect technologies.

The firm also tracks acquisitions within the connector space, conducts multi-client studies, and participates in customer specific research projects.

View other posts from Ronald E. Bishop.
News & Information

Listen to our new podcast, TTI Distribution Download! TTI Specialists, supplier partners and more share their expertise and insight on the electronics industry. 

Apple | Spotify | YouTube

Stay Updated