Transportation

Resources for the Automotive and Transportation Industries

The Future of Transportation is Now

In the not too distant future, transportation will become part of the Internet of Moving Things. Connected vehicles will meet Smart Cities, ships will be controlled remotely and GPS, wireless radio and computers will enable Positive Train Control. The intersection of technology and possibility pose demanding and interesting design challenges. From sensors to vehicle electrification, from design to production, on-board and off-board – a TTI Transportation Specialist will help you keep moving into the future. TTI has been successful for over 40 years for two fundamental reasons:  the industry's broadest and deepest interconnect, passive and electromechanic inventory, and the specialists who know all about it. 

Electrification

Most electric motors are designed to be efficient at generating torque and horsepower and, as a result, are not as symmetrical as they could be as if they were designed to be generators as well. The regenerative braking energy needs to mate well with the battery charging technology and while battery technology is changing, regenerative braking is getting better.

Manufacturers are now designing modern electric motors for use with hybrid vehicles. Expect performances up to 2500 Newton-Meter torque ratings and 8000 RPM rotational speeds. Established motor companies have these capabilities, as well as the ability to design custom motor/generators. Keep in mind that costs must be kept low. 

Power electronics are key. Whether acting as traction motors or generator brakes, ultra-low resistance connectivity, cabling, and electrical control systems for loads like 1200A of currents are not trivial, especially when the working voltages can range from 24 to 750V DC or more. Excerpted from: Not Your Daddy's Hybrid: Next Generations Rival the Best, by Jon Gabay for Mouser Electronics.

While aspects of vehicle electrification may seem fad-like with limited impact, electric vehicles themselves are well on their way to commercial acceptance. They are seen as a mature solution to reducing green-house-gases, pollutants and traffic in densely populated areas. Whether we like it or not, fossil fuels are finite – there is a future where they will no longer exist for transportation as we see it, electrification can improve this prediction today.

Autonomous Driving

Like it or not, self-driving vehicles in one form or another represent the future of automotive transportation, potentially saving lives and allowing many more vehicles to share a crowded highway system. As self-driving vehicles mature, the technologies that will control and sense the world around these vehicles remain in question. LIDAR – a combination of light and radar – has come to dominate this discussion, with a wide range of supporters but with one very notable detractor.

LIDAR works similarly to radar systems. Instead of a radar wave, it shoots focused laser beams into its environment and measures the time the reflection takes to return. With this data, it then obtains a point cloud of the surrounding area, letting the autonomous vehicle “see” its surroundings, not as an image but as a 3D model—as if creating a video-game-world based on the car’s surroundings, with the car itself inside.

Other technologies attempt to imbue vehicles with the same perception but do so with different technologies such as vision sensors (cameras), ultrasound sensors, and radar. Each of these has advantages and disadvantages.

Excerpted from: Almost Everyone Thinks LIDAR is the Technology Choice for Self-Driving Cars, by Jeremy Cook for Mouser Electronics

Connected Vehicle

Emerging trends highlight the role of the connected vehicle in transportation, but vehicles are poised to become an essential platform for personal mobility. In combination with personal electronics, the connected vehicle will redefine the mobile experience, bringing the separate capabilities of mobile device and vehicle together into a single, safe, personalized environment. 

Some of the most promising opportunities for extending mobile-device functionality lie in the ability of connected vehicles to use their powerful resources to complement these devices for services such as navigation. Vehicles can take advantage of their size and ready power sources to provide a more sensitive signal-reception platform or complement that platform with advanced inertial measurement unit (IMU) devices able to track location in the absence of GPS signals. Similarly, connected vehicle platforms can offer resources to buffer large data sets such as detailed route maps—both speeding performance and filling in data gaps found in GPS or cell coverage. Just as important, vehicle platforms can support the additional navigation-design complexity required to resist accidental or intentional interference including navigational signal spoofing.

Excerpted from: How Connected Vehicles Will Safely Leverage Smartphones, by Stephen Evanczuk for Mouser Electronics

Rugged Vehicles

The commercial vehicle market consistently requires stronger defenses against hazards such as temperature, vibration, and exposure to moisture or chemicals, all of which can cause failure. As a result, suppliers are developing ruggedized connectors that meet stringent requirements and ratings. Connector manufacturers are taking advantage of slower demand in the heavy-duty Class 8 truck and bus markets to make significant investments in new product development, aggressively going after market share and preparing for a market uptick by introducing forward-thinking products. At the center of most of this innovation is harsh environment performance.       

Excerpted from: Connector Innovations for Commercial Vehicles, by Lee Iken for TTI Inc.

Rail & Transit

Whether designing for the transportation of passengers or freight by bus, light rail, heavy rail, commuter rail, or steamship – safety, cost efficiency and reliability are paramount. Today’s passengers expect interlinked mobility chains and payment systems and virtual real-time scheduling. Freight owners require real asset tracking. New rail designs incorporate the latest technological innovations such as microprocessor-controlled brake and propulsion systems, data bus configuration for information and control transfer between cars, an onboard microprocessor maintenance diagnostic system, digital controlled voice and signage, and positive train control compliance. Remaining competitive in this market is complex and requires the application of leading edge electronic component technology, interconnect systems and electromechanical devices.

Line Cards & More Info

Featured Suppliers