This is what's Keeping Electric Planes from Taking Off
8/17/2022 // By Casey Crownhart
Startups are exploring how electric planes could clean up air travel, which accounts for about 3% of worldwide greenhouse-gas emissions. The problem is that today’s electric aircraft could safely carry you and about a dozen fellow passengers only around 30 miles, according to a recent analysis.
The limiting factor is the battery, in particular the amount of energy that can be stored in a small space. If you’ve folded your legs into a cramped window seat or been charged extra for overweight luggage, you’re probably familiar with the intense space and weight constraints on planes.