TE Connectivity I/O Module
The I/O system (or Remote I/O) provides the physical connection between devices and PLC’s and therefore allow a closer control at the factory floor. I/O modules are growing in popularity as they provide flexible and fast reconfiguration of sensor-level networks without the need for panels and cabinets. TE connectivity offers innovative interconnect solutions that allow for reliable, uninterrupted industrial communication allowing I/O systems to fully control the factory floor.
Request a Hard Copy:
Customers in the Americas
can request a free hard copy
of this publication (while supplies last).