AN11599 Using Power MOSFETs in Parallel

Nexperia AN11599 Using Power MOSFETs in Parallel explores some of the problems that can be experienced when several MOSFETs are operated in a paralleled group. These increase the capability of a MOSFET switch element by using several individual MOSFETs connected in parallel can be useful. However, when designing switch elements careful consideration of the circuit requirements and the MOSFET characteristics and behavior must be applied. Learn more about ways to avoid these problems and minimize their effects.

Search All Nexperia MOSFET