Nexperia Addressing Floating Inputs In Digital Systems
Nexperia Addressing floating inputs in digital systems defines in the normal operations of a digital system that the input to any digital device within is clearly defined - it is either one or zero. There are interface cases where outputs may be disabled which can result in floating inputs.