Littelfuse Flow Sensing in Tankless Water Heaters

Tankless water heaters are a popular solution for water heating needs. The availability of hot water on demand and the perceived limitless supply of hot water make these types of water heaters much more attractive than traditional tank water heaters. These water heaters also provide long-term energy savings since energy is used only when there is a demand for hot water. In order to effectively heat the water when there is a demand, a sensor is needed to detect the flow of water. Learn more about Littelfuse reed switches and proximity sensors functionality in applications that use tankless water heaters.

Search all Littelfuse Magnetic / Reed Switches and Proximity Sensor products.