AEC-Q200 Qualified Fuses NPI Presentation

Littelfuse cartridge fuses (526, 527, and 828 Series) are designed and tested to meet the new test requirements as specified in the new AEC-Q200 revision. These robust fuses from Littelfuse include a range from 500 to 1000 Vdc rating and provide an excellent interrupting rating. These fuses are ideal for the On-Board Chargers (OBCs) and Power Distribution Units (PDUs) in the latest electric vehicle designs. 

Search All Littelfuse Cartridge Fuses including the 526 Series, 527 Series, and 828 Series