Honeywell Inspection of Oil Filters
The ultrasonic sensor is not affected by the shine of the metal. Both sides of the spacer target present a good flat target for the sensor. The narrow beam diameter of the sensor when operated in the maximum rate mode is only 6 degrees. Therefore, the sensor can send the ultrasonic beam down the inside of the filter element without getting any interference from the side walls of the element.