AN-014 Contact Welding Application Note

GIGAVAC performs extensive testing to determine the current capability of its contractors. In applications where contact welding occurs almost every case can be attributed to either the coil drive circuit or underestimating the make load current. Higher load currents are usually from load capacitance. Learn more about GIGAVAC contactors in this application note.

Search All GIGAVAC Contactors