Bourns Selecting the Appropriate Position Feedback Sensor for Factory Automation Valve Designs

An integral part of automating factory equipment is the ability to read and monitor the real-time position of valves. Programmable Logic Controllers (PLCs) and Input/Output (I/O) modules are now being implemented in factory machinery to transmit valuable information on valve adjustment based on the actual position provided by the position feedback sensor.