Fort Worth, Texas – March 7, 2023 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the CNY66 family of High Voltage Optocouplers from Vishay. These devices are targeted to meet the requirements of various high voltage isolation applications. Vishay’s CNY66 Series consists of a phototransistor optically coupled to a gallium arsenide infrared-emitting diode in a 4-pin plastic package. The single components are mounted opposite one another, providing a distance between input and output for highest safety requirements of > 3mm. Special features includerated recurring peak voltage (repetitive) VIORM = 1450 Vpeak, thickness through insulation ≥ 3 mm and creepage current resistance according to VDE 0303/IEC 60112. These optocouplers are AECQ-101 qualified for robust performance in automotive and industrial applications.
To learn more, visit: Vishay High Voltage Optocouplers | TTI, Inc.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com.
About Vishay Semiconductor
Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader.