Fort Worth, Texas – October 13, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is stocking API Technologies’ Hermetically Sealed Threaded Case Filters with QPL’s for the MIL-F-15733, MIL-F-28861 and DSCC 84084.

This series of filters features hermetic glass seals and high EMI filtering performance. They are excellent for critical applications that demand high reliability in the toughest environmental conditions and provide broadband high performance EMI filtering from 10KHz to over 10GHz.
Available in the popular case diameters of .375", .410" and .690", they are offered in voltage ratings from 50V to 400VDC/240AC, 400Hz and are impervious to high moisture and humidity environments, solvents and severe environmental conditions such as high frequency vibration, high levels of shock and extreme temperatures.

To learn more, visit: Hermetically Sealed Threaded Case Filters  | TTI, Inc.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About API Technologies
APITech (API Technologies Corp.) is an innovative designer and manufacturer of high-performance subsystems, modules, and components to Protect, Power, and Process critical RF and electronics applications. A high-reliability technology pioneer with over 70 years of heritage, APITech's products are used by global defense, industrial, and commercial customers for critical applications including electronic warfare, Radar, C4ISR, Space, missile defense, commercial aerospace, wireless communications, medical, oil and gas, and harsh environments.