Fort Worth, Texas – October 7, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking Dialight 558 Green Snap-In Panel Mount Indicators. These indicator lights are designed to meet the indication requirements of a variety of communications and networking equipment applications.
Dialight’s 558 Green Series LED Snap-In Panel Mount Indicators, featuring bi-color and integral resistors, are available in a variety of lead lengths for high-brightness applications. These high- quality, long-life LEDs are easy to install and are designed for applications such as fan tray assemblies, data center servers and storage infrastructure, networking equipment (such as switches and routers) and electronic test and measurement. They are available with straight terminals for wire wrapping, soldering or 26 AWG lead wires and include a wide operating temperature range of -55°C to +100°C for excellent harsh environment performance.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Dialight
Dialight is the world leader in LED technology with millions of LED fixtures and indicators installed worldwide. The company began in 1938 in Brooklyn, NY, where they produced instrument panel lights for aircraft. In 1971 Dialight launched the first LED Circuit Board Indicators. Dialight has revolutionized the use of LEDs to provide superior lighting for traffic control, indicators, structural towers and industrial sites around the world.