Fort Worth, Texas – October 6, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking ACSA 02 Series Numeric Displays from Kingbright. These highly efficient SMD devices are well suited for display applications in medical, commercial and industrial test and measurement equipment. 

Kingbright’s highly efficiency displays are available in popular colors including red, green, amber, orange and several other options. Kingbright continues to advance its SMD display products by developing the ultra-thin, 0.8”-character-height ACSA 02 Series SMD Numeric Display with thickness as thin as 0.12” (3mm). This remarkable characteristic enhances design flexibility and readout clarity for engineers and designers in various appliance and healthcare applications. Furthermore, this SMD display’s lightweight and low profile design coupled with its vivid and crisp displaying capability make handheld testing devices, instrumental equipment and consumer electronics smaller, lighter and flashier.

Kingbright offers an extensive selection of SMD displays including sizes in 0.2”, 0.3”, 0.4”, 0.56” 0.8” and colors such as blue (470nm), green (570nm), red (635nm), yellow (590nm) and orange (601nm). In addition, this item is available in different types consisting of single/dual digit as well as alphanumeric. The SMD Display’s automation-friendly tape and reel package and robust design reduce assembly cost and eliminate product deterioration during harsh assembly environment. 

To learn more, visit  Kingbright SMD Numeric Displays | TTI Inc.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About Kingbright
Kingbright Company LLC has manufactured innovative Light Emitting Diodes for over 30 years. Kingbright offers the most comprehensive LED product portfolio in the industry, including SMD LEDs, thru-hole LEDs, SMD/through-hole displays, circuit board indicators and high brightness LEDs. Kingbright also offers fully customized LED solutions to enhance customer designs with many options in LED packaging and colors.