Fort Worth, Texas – May 12, 2022 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of Amphenol Minitek® Pwr CEM-5 PCIe® Connector System from stock at TTI.

The Amphenol FCI Minitek Pwr CEM-5 PCIe Connector Systems provide a high current rating of up to 9.5A/pin (12 pins energized) and the four signal pins support signal transmission. These devices are designed with a 12VHPWR auxiliary hybrid connector and cable assembly that supports the 600W GPU cards. The 12VHPWR connector is not designed to mate with legacy PCI Express 2x3 and 2x4 12V auxiliary power connectors. The 12VHPWR connector power pins have a 3.00mm pitch, while the contacts in a legacy 2x3 and 2x4 connector lie on a larger 4.20mm pitch.

Typical applications include communications, networking and server/storage, to name a few. They are in stock and available today at TTI.

To learn more, visit Minitek Pwr CEM-5 PCIe Connector Systems from TTI, Inc.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com