Fort Worth, Texas – May 10, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the ROHM SLA-570MT Series of green through-hole 5mm LEDs. These high-output LEDs are designed with epoxy resin lenses to optimize color efficiency. This new lineup includes options in 220 to 1000mcd bins. LEDs are optimized for uses in digital signage, industrial and medical indication applications.

The ROHM SLA-570MT Series LEDs are high-intensity devices designed for color and indicator applications. Offered in an industry-standard 5mm through-hole package for manufacturing ease, this product is well suited for digital signage where high component density is required. It also features design flexibility for indication and backlighting in medical devices and other handheld mobile devices where low power consumption is desirable. ROHM’s new product is compatible with standard soldering processes, environmentally friendly, RoHS compliant and halogen-free.

View all ROHM Semiconductor products.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About ROHM Semiconductor
ROHM offers a full line of leading-edge sensors, silicon carbide MOSFETs and Schottky barrier diodes, optoelectronics, and power management ICs. If you’re designing for rugged environments requiring high-temperature and/or high-voltage along with higher power density solutions – TTI is fully franchised for ROHM, Kionix MEMS Sensors and accelerometers, and LAPIS Semiconductor products.