Fort Worth, Texas – March 29, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking Dialight’s 558 Snap-In Panel Mount Indicators. These LED indicator lights are designed to fulfill the indication requirements of a variety of industrial, communications and networking equipment applications.

Dialight’s 558 Series LED Snap-In Panel Mount Indicators are available in a variety of LED colors for high brightness applications, bi-color and integral resistors. These easy-to-install indicators are designed for applications such as fan tray assemblies, data center servers and storage infrastructure, networking equipment (such as switches and routers) and electronic test and measurement. Available with straight terminals for wire wrapping, soldering or 26 AWG lead wires, these indicators feature a wide operating temperature range of up to -55°C to +100°C for harsh environment requirements.

View all Dialight products.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About Dialight
Dialight is the world leader in LED technology with millions of LED fixtures and indicators installed worldwide. The company began in 1938 in Brooklyn, NY, where they produced instrument panel lights for aircraft. In 1971 Dialight launched the first LED Circuit Board Indicators. Dialight has revolutionized the use of LEDs to provide superior lighting for traffic control, indicators, structural towers and industrial sites around the world.