Fort Worth, Texas – March 24, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the VCNL4200 family of Proximity Sensors from Vishay. These sensors are targeted to meet the requirements of medical, process automation and industrial sensing applications.
Vishay’s VCNL4200 integrates a high-sensitivity long-distance proximity sensor (PS), ambient light sensor (ALS) and 940nm IRED into one small package. It incorporates photodiodes, amplifiers and analog-to-digital converting circuits into a single chip using the CMOS process. The 16-bit high-resolution ALS offers excellent sensing capabilities with sufficient selections to fulfill most applications, whether using a dark or high transparency lens design. VCNL4200 offers individual programmable high and low threshold interrupt features for the best utilization of resources and power saving on the microcontroller. For the 12-bit/16-bit proximity sensing function, VCNL4200 has a built-in intelligent cancellation scheme that eliminates background light issues. The persistence feature prevents false judgment of proximity sensing due to ambient light noise.
To learn more, visit Vishay VCNL4200 Proximity Sensors at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Vishay Semiconductor
Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader.