Fort Worth, Texas – March 24, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now offering the SIR-563ST3F family of Infrared LEDs from ROHM Semiconductor. These emitters are designed for specialty infrared illumination and sensing applications such as medical instruments, industrial and manufacturing automation, safety and security equipment.

ROHM’s SIR-563ST3F family of Infrared Emitters is uniquely suited for specialty sensing of movement or presence in limited spacing applications and features a highly efficient LED die for maximum IR power in low voltage and battery-powered products. These devices, which include a built-in, 15-degree emission half-angle, have an operating temperature range from -40°C to +85°C for industrial product operation.

To learn more, visit ROHM Infrared Emitters at TTI.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About ROHM Semiconductor
ROHM offers a full line of leading-edge sensors, silicon carbide MOSFETs and Schottky barrier diodes, optoelectronics, and power management ICs. If you’re designing for rugged environments requiring high-temperature and/or high-voltage along with higher power density solutions. ROHM’s product family includes ROHM Semiconductor, Kionix MEMS Sensors and accelerometers, and LAPIS Semiconductor products.