Fort Worth, Texas – March 16, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is stocking Military Established Reliability qualified to MIL-PRF-55182/9 Resistors from Vishay Foil Resistors (VFR). These high-reliability resistors are available in resistance values from 4.99Ω through 121kΩ and with tolerances from ±0.005 to ±1.0 percent, applicable for your long-range navigation equipment, military and aerospace projects.
The RNC90Y/Z can handle unconventional environmental conditions above and below the surface with minimal drift. It provides high resistance to thermal shock, moisture, mechanical shock and vibrations and features tin/lead alloy terminations. Sample quantities are available.
View all Vishay Precision Group products.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Vishay
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors, passive electronic components and circuit protection devices that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.™ Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH).