Fort Worth, Texas – March 16, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the RPR-220 Reflective Optical Sensor Series from ROHM Semiconductor. This sensor is targeted for specialty sensing applications, including medical, industrial, manufacturing automation, safety and security equipment.

ROHM’s RPR-220 family of compact, through-hole, reflective sensors are packaged in a rugged opaque plastic housing with an integrated 940nm LED and phototransistor for optimum sensing performance. The LED can be driven at 50mA with 80mW power dissipation, and the detector operates at 5V and produces a minimum collector current of 0.8mA. Response times are rated at 10ms for high-speed detection and time-critical applications. The ideal object detection distance is 6mm. The operating temperature range is from -25 to +85°C. This device is designed for critical sensing in factory automation, robotics and handheld equipment applications.

View all ROHM Semiconductor products.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About ROHM Semiconductor
ROHM offers a full line of leading-edge sensors, silicon carbide MOSFETs and Schottky barrier diodes, optoelectronics, and power management ICs. If you’re designing for rugged environments requiring high-temperature and/or high-voltage along with higher power density solutions – TTI is fully franchised for ROHM, Kionix MEMS Sensors and accelerometers, and LAPIS Semiconductor products.