Fort Worth, Texas – March 14, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the TFDU4101 family of Transceiver Modules from Vishay. These devices are targeted to meet the communication requirements of various medical, networking and industrial applications.

Vishay’s TFDU4101 Transceiver is an infrared transceiver module compliant to the latest IrDA® physical layer standard for fast infrared data communication, supporting IrDA speeds up to 115.2 kbit/s (SIR) and carrier based remote control modes. Integrated within the transceiver module are a photo pin diode, an infrared emitter (IRED) and a low-power control IC to provide a total front-end solution in a single package. This device covers the full IrDA range of more than 1 meter using the internal intensity control. With one external current control resistor, the current can be adjusted for shorter ranges, saving operating current in the IrDA low-power mode. TFDU4101 has a tristate output and is floating in shutdown mode with a weak pull-up. These devices are used in medical data collection, networking, data logging, POS systems and portable computers.
.
To learn more, visit Vishay IrDA Transceivers at TTI.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About Vishay Semiconductor
Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader.