Fort Worth, Texas – March 14, 2022 – TTI, Inc., a leading specialty distributor of electronic components, now offers the ROHM BD8379FV-M LED Driver Series. These highly integrated 12-channel drivers are optimized for signage and illumination applications requiring precise control of color, uniformity and intensity.

ROHM’s BD8379FV-M is a serial-in, parallel-out controlled LED driver with a 35V output voltage rating. Offered in an SSOP-B20 SMT package with the inputs of 3-line serial data, it turns the 12-channel open drain output on and off. Due to its compact size, it is optimal for limited space applications. Key features include open drain output, 3-line serial control and enable signal along with cascade connection compatibility and an internal 12-channel power transistor for added functionality. These LED drivers are AEC-Q101 qualified, making them suitable for medical and automotive applications demanding increased reliability.

View all ROHM Semiconductor products.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About ROHM Semiconductor
ROHM offers a full line of leading-edge sensors, silicon carbide MOSFETs and Schottky barrier diodes, optoelectronics, and power management ICs. If you’re designing for rugged environments requiring high-temperature and/or high-voltage along with higher power density solutions.