Fort Worth, Texas – March 7, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking Dialight’s 596-1616-013F Prism® IceBlue LED Circuit Board Indicators. These small form factor indicator lights are designed to meet the unique requirements of interface cards, networking and test equipment applications.
Dialight’s 596-1616-013F Prism LED Circuit Board Indicators are the small, right-angle indicators for precision electronics. The Prism Series is available in a variety of package sizes including single level, bi-level and tri-level configuration and in 2mm and 3mm lens sizes. These LED indicators are designed to withstand 260°C peak reflow temperature and provide the aesthetics of a diffused lens for better visibility. They provide a dominant wavelength of 470nm and a wide range of intensities. These LED indicators feature proprietary design for SMT applications, board-edge mounting in network interface cards, networking hardware, wireless components, electronic testing and measuring equipment.
To learn more, visit Dialight Bi-Level Indicators at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Dialight
Dialight is the world leader in LED technology with millions of LED fixtures and indicators installed worldwide. The company began in 1938 in Brooklyn, NY, where they produced instrument panel lights for aircraft. In 1971 Dialight launched the first LED Circuit Board Indicators. Dialight has revolutionized the use of LEDs to provide superior lighting for traffic control, indicators, structural towers and industrial sites around the world.