Fort Worth, Texas – March 2, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking Dialight’s 515-1071 Series Light Pipes. These light pipes are designed to utilize a PLCC 2 or PLCC 4 PCB-mounted LED for ideal light transmission.

Dialight’s Optopipe® 515-1071F circular light-emitting surfaces appear bright and uniform in intensity. They are reliably held in place by two press-fit pins located on the right side of each of the two light pipe elements. These Optopipes function as a through-the-case indicator with a textured finish on the two light-emitting surfaces that increases its viewing angle. The recommended light sources are Dialight's 597 Series PLCC-2 or PLCC-4 Type SMT LEDs. The LEDs are mounted in a straight line on a 0.250” pitch. The light pipe material is water-clear, transmissive-polycarbonate-rated UL94-V0 and has a 35 percent oxygen index.

To learn more, visit Dialight Two Position Light Pipes at TTI.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About Dialight
Dialight is the world leader in LED technology with millions of LED fixtures and indicators installed worldwide. The company began in 1938 in Brooklyn, NY, where they produced instrument panel lights for aircraft. In 1971 Dialight launched the first LED Circuit Board Indicators. Dialight has revolutionized the use of LEDs to provide superior lighting for traffic control, indicators, structural towers and industrial sites around the world.